Snap Buttons

Filter

VALCO VALLEY TOOL AND DIE -

Steel Snap Buttons

StyleModelTypeWidthGaugeHead HeightHead Dia.Round Tubing Inside Dia.Square Tubing Inside Dia.MaterialPrice (ex. VAT)Pkg. Qty.
AD150Double End11/25"0.02 ga.0.37"0.312"0.82" to 1.12"0.82" to 1.12"Steel€12.535
AD182Double End0.53"0.025 ga.11/25"3/8"1" to 1.87"1" to 1.87"Steel€30.245
AD181Double End0.53"0.025 ga.0.37"3/8"0.87" to 1.87"0.87" to 1.87"Steel€30.245
AD131Double End0.365"18 ga.7/25"1/4"0.62" to 0.87"0.62" to 0.87"Steel€11.115
BE140Dual11/25"0.02 ga.0.37"0.302"0.52" to 1"0.52" to 1"Steel€44.765
BE130Dual0.35"0.018 ga.7/25"6/25"0.5" to 0.75"0.44" to 0.75"Steel€34.205
CA134Single End0.35"0.018 ga.0.39"1/4"0.5" to 1.25"0.42" to 1.25"Steel€26.4110
DB180Single End0.51"0.025 ga.0.37"3/8"0.62" to 1.12"0.52" to 1.12"Steel€26.0410
CA161Single End0.51"-0.37"0.365"0.68" to 1.37"0.52" to 1.37"Steel€30.6610
CA180Single End0.51"0.025 ga.0.37"3/8"0.7" to 1.37"0.55" to 1.37"Steel€30.6610
DB134Single End0.35"20 ga.0.39"1/4"0.55" to 1"0.55" to 1"Steel€26.4110
DB130Single End0.365"0.018 ga.7/25"1/4"0.45" to 0.8"0.37" to 0.8"Steel€17.8510
CA130Single End0.365"0.018 ga.7/25"1/4"0.45" to 0.87"0.42" to 0.87"Steel€17.2310
DB150Single End11/25"0.02 ga.0.37"0.312"0.55" to 1"0.45" to 1"Steel€26.4110
CA170Single End0.53"0.025 ga.0.37"0.365"1.25" to 1.75"1.12" to 1.75"Steel€33.5010
CA150Single End11/25"0.02 ga.0.37"0.312"0.59" to 1.25"0.49" to 1.25"Steel€21.0010
VALCO VALLEY TOOL AND DIE -

Stainless Steel Snap Buttons

StyleModelWidthGaugeHead HeightHead Dia.Round Tubing Inside Dia.Square Tubing Inside Dia.TypeMaterialPrice (ex. VAT)Pkg. Qty.
AII1500.312"0.025 ga.0.37"0.312"0.55" to 1"0.5" to 1"Single EndStainless Steel€54.055
AII1320.312"0.025 ga.0.37"1/4"0.57" to 0.87"0.43" to 0.87"Single EndStainless Steel€46.935
AII1301/4"0.022 ga.7/25"1/4"0.43" to 0.87"0.41" to 0.87"Single EndStainless Steel€46.135
AII1803/8"0.03 ga.0.37"3/8"0.6" to 1.12"0.55" to 1.12"Single EndStainless Steel€59.005

Snap Buttons

These snap buttons are widely used in wheelchairs, portable toilets, crutches, electrical transformers, telescoping poles, banner stands, kiosks, fishing equipment, soccer & hockey goals and pop-up tents. They are also used to attach fabric to solid surfaces such as plastic, cardboard or wood.

Frequently Asked Questions

What is a snap button barrel?

It is the stem-like part of the snap button that is riveted into the mating component. It extrudes out of the backside of the button top.

What causes snaps to stop holding?

A snap's stud (bottom) is frequently fastened to a solid surface, such as the side of a boat. It supports the socket (top), which is riveted to the button cap's underside. A taut wire spring that surrounds the stud as it is put on and lifted off, is located inside the socket. Over time, the spring loses strength, leading to the fastener's failure.

How do you stabilise snaps?

For stabilising, a sew-in material such as a non-fusible or woven interfacing, similar-weight cotton fabric or twill tape can be used.

Can you reuse snap buttons?

Do not reuse snap parts as they get damaged. Throw them and start with new parts.

How to replace worn-out snaps?

  • Determine the type and size of the existing snaps.
  • Remove the old socket by drilling off the rivet with a drill from the rolled side of the rivet.
  • Install the new socket with a snap fastener installation tool.

What is the significance of a snap button closure?

A snap closure uses snap fasteners, which are essentially two discs that fit together like snug jigsaw pieces. One disc has a projecting end, and the other is concave.

We are here to help!

Looking for a part not listed here?