Left Hand Inserts

Filter

Left-hand inserts are ideal for repairing stripped threads or creating new threads in a drilled hole to install left-hand threaded fasteners. Raptor Supplies offers these left-hand inserts...Read more

StyleModelMPN
A86116LH86116LH
RFQ
A86117LH86117LH
RFQ
A86118LH86118LH
RFQ
A86119LH86119LH
RFQ
A86120LH86120LH
RFQ
A86121LH86121LH
RFQ
A86122LH86122LH
RFQ
A86123LH86123LH
RFQ
A86124LH86124LH
RFQ
A86126LH86126LH
RFQ
A86129LH86129LH
RFQ
A86130LH86130LH
RFQ
A86131LH86131LH
RFQ
A86132LH86132LH
RFQ
A86133LH86133LH
RFQ
A86134LH86134LH
RFQ
A86135LH86135LH
RFQ
A86137LH86137LH
RFQ
A86157LH86157LH
RFQ
A86159LH86159LH
RFQ
A86160LH86160LH
RFQ
A86164LH86164LH
RFQ
A86165LH86165LH
RFQ
A86169LH86169LH
RFQ
A86171LH86171LH
RFQ
CHRISLYNN -

Imperial Precision Standard Industrial Kit

Left-hand inserts are ideal for repairing stripped threads or creating new threads in a drilled hole to install left-hand threaded fasteners. They provide more strength, versatility & resilience than the fasteners installed inside traditional threaded holes. These inserts have left-handed threads (also called reverse threads) for specialised applications like automotive, heating & plumbing pipes and gas supply valves, where right-hand threaded fasteners would loosen due to pressure.
These inserts have widely spaced threads to start tightening easily.

StyleModelLengthThread SizeThread Type
A82124LH3/4"1/2"-13Coarse
RFQ
A82116LH3/8"1/4"-20Coarse
RFQ
A82120LH9/16"3/8"-16Coarse
RFQ
A82118LH15/32"5/16"-18Coarse
RFQ
A82122LH21/32"7/16"-14Coarse
RFQ
CHRISLYNN -

Stainless Steel Left Hand Insert Kits

StyleModelLengthThread SizeThread TypeMaterialPrice (ex. VAT)
A82137LH1 1/2"1"-14FineStainless Steel€728.76
A82135LH1 1/2"1"-8CoarseStainless Steel€728.76
B82132LH1 1/8"3/4"-16FineStainless Steel€443.24
B82131LH1 1/8"3/4"-10CoarseStainless Steel€397.89
A82134LH1.312"7/8"-14FineStainless Steel€521.69
A82133LH1.312"7/8"-9CoarseStainless Steel€521.69
B82126LH3/4"1/2"-20FineStainless Steel€277.41
C82117LH3/8"1/4"-28FineStainless Steel€219.08
C82157LH9 mmM6MetricStainless Steel€267.66
C82121LH9/16"3/8"-24CoarseStainless Steel€225.43
C82160LH12 mmM8MetricStainless Steel€282.63
C82159LH12 mmM8MetricStainless Steel€282.33
C82165LH15 mm-MetricStainless Steel€289.25
C82164LH15 mmM10MetricStainless Steel€288.00
B82130LH15/16"5/8"-18CoarseStainless Steel€287.34
B82129LH15/16"5/8"-11CoarseStainless Steel€277.12
C82119LH15/32"5/16"-24FineStainless Steel€225.43
D82171LH18 mmM12 x 1.75MetricStainless Steel-
RFQ
B82169LH18 mmM12 x 1.25MetricStainless Steel€337.42
B82173LH21 mmM14MetricStainless Steel€435.61
B82172LH21 mmM14MetricStainless Steel€435.61
B82123LH21/32"7/16"-20FineStainless Steel€302.94
B82175LH24 mmM16MetricStainless Steel€476.52
B82174LH24 mmM16MetricStainless Steel€478.58
B82178LH27 mmM18MetricStainless Steel€470.78
StyleModelLengthThread SizeThread TypeMaterialPrice (ex. VAT)Pkg. Qty.
A83135LH1 1/2"1"-8CoarseStainless Steel€128.002
A83137LH1 1/2"1"-14FineStainless Steel€128.002
A83132LH1 1/8"3/4"-16FineStainless Steel€78.372
A83131LH1 1/8"3/4"-10CoarseStainless Steel€78.372
A83133LH1.312"7/8"-9CoarseStainless Steel€95.632
A83134LH1.312"7/8"-14FineStainless Steel€95.632
A83124LH3/4"1/2"-13CoarseStainless Steel€112.194
A83126LH3/4"1/2"-20FineStainless Steel€112.194
A83116LH3/8"1/4"-20CoarseStainless Steel€159.646
A83117LH3/8"1/4"-28FineStainless Steel€159.646
A83157LH9 mmM6 x 1MetricStainless Steel€159.646
A83121LH9/16"3/8"-24FineStainless Steel€159.646
A83120LH9/16"3/8"-16CoarseStainless Steel€159.646
A83159LH12 mmM8 x 1MetricStainless Steel€159.646
A83160LH12 mmM8 x 1.25MetricStainless Steel€159.646
A83165LH15 mmM10 x 1.5MetricStainless Steel€168.416
A83164LH15 mmM10 x 1.25MetricStainless Steel€168.416
A83130LH15/16"5/8"-18FineStainless Steel€64.502
A83129LH15/16"5/8"-11CoarseStainless Steel€64.502
A83118LH15/32"5/16"-18CoarseStainless Steel€159.646
A83119LH15/32"5/16"-24FineStainless Steel€159.646
A83171LH18 mmM12 x 0.75MetricStainless Steel€192.506
A83169LH18 mmM12 x 1.25MetricStainless Steel€192.506
A83173LH21 mmM14 x 2MetricStainless Steel€192.506
A83172LH21 mmM14 x 1.5MetricStainless Steel€192.506

Left Hand Inserts

Left-hand inserts are ideal for repairing stripped threads or creating new threads in a drilled hole to install left-hand threaded fasteners. Raptor Supplies offers these left-hand inserts from Chrislynn. They provide more strength, versatility & resilience than the fasteners installed inside traditional threaded holes. They have left-handed threads (also called reverse threads) for specialised applications like automotive, heating & plumbing pipes and gas supply valves, where right-hand threaded fasteners would loosen due to pressure.

Frequently Asked Questions

Why are left-hand inserts larger in diameter than the tapped hole before installation?

Left-hand inserts feature a slightly larger diameter compared to the tapped hole diameter before installation, as the leading coil's diameter decreases when the installation tool applies torque to the insert's prong / tang. After these threaded inserts get installed, they act as a spring to expand outward onto the material and provide strong anchoring.

Why do these left-hand inserts have open ends?

These inserts have an open end for allowing the installation of fasteners with a longer length than them.

What accessories are compatible with these left-hand inserts?

Installation of these left-hand inserts requires a drill bit, a tapping tool, an installation tool and a prong break-off tool. Selected models come in a kit containing all these tools.

How to determine the length of the left-hand insert required?

  • Length of a helical left-hand insert should be at least as long as the desired screw diameter. Users may choose longer inserts for increased strength.
  • The exact insert length can vary depending upon the application & the material in which the insert is being installed. Hard materials like steel do not need long inserts. For soft materials like aluminium, a longer insert may be preferable.

How to install a helical left-hand insert?

  • Drill a hole according to the length of the insert / screw / bolt to be installed.
  • Thread the drilled hole using a tapping tool.
  • Thread the insert into the tapped hole using an installation tool by properly gripping the insert's prong.
  • Wind the insert inside the hole up to a quarter to half turn below the hole's surface.
  • Remove the prong using a prong break-off tool or punch to allow full passage of the fastener into the insert.

Can thread inserts be removed once installed?

Yes, some thread inserts can be removed using removal tools that attach to them & unwind them in the direction opposite to that used during installation.

We are here to help!

Looking for a part not listed here?