Anchor Setting Tools

Filter

Anchor setting tools are used to drive anchors in wood, concrete & other surfaces. These tools include anchor shackles, Con-Sert tools, driver tools, drop-in anchor setting tools,...Read more

StyleModelAnchor Dia.MaterialAnchor Tool TypePrice (ex. VAT)
A00429SD-PWR1/2"SteelDrop In Automatic Anchor Setting Tool€216.39
A00425SD-PWR1/4"-Drop In Automatic Anchor Setting Tool€190.70
A00427SD-PWR3/8"SteelDrop In Automatic Anchor Setting Tool€214.17
-

1/4"-20 Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialGradeThread SizeAnchor Tool TypePrice (ex. VAT)
ART-1141/4"Steel-1/4"-20Drop In Anchor Setting Tool€8.43
B13147001/4"SteelGrade 51/4"-20Drop In Anchor Setting Tool€6.59
-

5/8"-11 Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialGradeThread SizeAnchor Tool TypePrice (ex. VAT)
A13587005/8"SteelGrade 55/8"-11Drop In Anchor Setting Tool€12.26
BRT1585/8"Steel-5/8"-11Drop In Anchor Setting Tool€16.13
-

3/8"-16 Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialGradeThread SizeAnchor Tool TypePrice (ex. VAT)
ARTX-1383/8"Steel-3/8"-16Drop In Anchor Setting Tool€11.76
BRT1383/8"Steel-3/8"-16Drop In Anchor Setting Tool€8.98
C13387003/8"SteelGrade 53/8"-16Drop In Anchor Setting Tool€9.52
-

3/4"-10 Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialGradeThread SizeAnchor Tool TypePrice (ex. VAT)
ART1343/4"Steel-3/4"-10Drop In Anchor Setting Tool€20.62
B13347003/4"SteelGrade 53/4"-10Drop In Anchor Setting Tool€13.98
StyleModelAnchor Dia.MaterialThread SizeAnchor Tool TypePrice (ex. VAT)Pkg. Qty.
APSP50-G101/2"Steel1/2"-13Piloted Setting Punch€186.3010
APSP25-G101/4"Steel1/4"-20Piloted Setting Punch€110.1610
APSP37-G103/8"Steel3/8"-16Piloted Setting Punch€141.9310
-

Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialFinishAnchor Tool TypePrice (ex. VAT)
A06336-PWR-Steel-Drop In Anchor Setting Tool€14.41
B09353-PWR1/2"SteelZinc PlatedDrop In Anchor Setting Tool€150.00
C09352-PWR1/2"SteelZinc PlatedDrop In Anchor Setting Tool€58.62
D06309-PWR1/2"Steel-Drop In Anchor Setting Tool€14.27
A06338-PWR1/2"Steel-Drop In Anchor Setting Tool€26.49
E06305-PWR1/4"Steel-Drop In Anchor Setting Tool€5.52
B09323-PWR1/4"SteelZinc PlatedDrop In Anchor Setting Tool€112.95
C09322-PWR1/4"SteelZinc PlatedDrop In Anchor Setting Tool€49.04
F06313-PWR3/4"Steel-Drop In Anchor Setting Tool€21.65
GPFM21017203/8"Steel-Drop In Anchor Setting Tool€54.52
F06307-PWR3/8"Steel-Drop In Anchor Setting Tool€7.77
A06323-PWR3/8"Steel-Drop In Anchor Setting Tool€14.14
B09343-PWR3/8"SteelZinc PlatedDrop In Anchor Setting Tool€134.38
B09363-PWR5/8"SteelZinc PlatedDrop In Anchor Setting Tool€230.55
D06311-PWR5/8"Steel-Drop In Anchor Setting Tool€13.09
C09362-PWR5/8"SteelZinc PlatedDrop In Anchor Setting Tool€242.55
C09342-PWR5/16"SteelZinc PlatedDrop In Anchor Setting Tool€48.83
B09333-PWR5/16"SteelZinc PlatedDrop In Anchor Setting Tool€97.27
GREENLEE -

Screw Anchor Expander Anchor Setting Tools

StyleModelAnchor Dia.MaterialThread SizeAnchor Tool TypePrice (ex. VAT)
A8681/4"Steel1/4"-20Screw Anchor Expander€244.97
B8703/8"Steel3/8"-16Screw Anchor Expander€345.06
-

1/2"-13 Drop-In Anchor Setting Tools

StyleModelAnchor Dia.MaterialGradeThread SizeAnchor Tool TypePrice (ex. VAT)
A13127001/2"SteelGrade 51/2"-13Drop In Anchor Setting Tool€10.68
BRTX-1121/2"Steel-1/2"-13Drop In Anchor Setting Tool€17.24
CRT 1121/2"Steel-1/2"-13Drop In Anchor Setting Tool€12.22
TAPCON -

Driver Tool, Installation Tool, SS

ModelItemPrice (ex. VAT)
3103910AD6UGG€173.25
DEWALT -

Drop-in Anchor Setting Tool, 1/2 In Anchor Dia., Steel

ModelItemPrice (ex. VAT)
03790-PWRCG6MFZ€246.80
DEWALT -

Drop-in Anchor Setting Tool, 1/2 In Anchor Dia., SS

ModelItemPrice (ex. VAT)
08345-PWRCG6MME€348.95
See Details

Anchor Setting Tools

Anchor setting tools are used to drive anchors in wood, concrete & other surfaces. These tools include anchor shackles, Con-Sert tools, driver tools, drop-in anchor setting tools, screw anchor expanders & piloted setting punches. Raptor Supplies offers a wide range of these tools from brands like Red Head, Diversified Fastening Systems, Grainger, Greenlee, MKT Fastening, Powers Fasteners, Dewalt, Strong-Tie and Tapcon.

Frequently Asked Questions

What is an anchor shackle?

Anchor shackles have a circular bow. These shackles are side loaded or employed in sling-leg connections owing to their broad bow form. They can be used to attach various lifting slings, chains or ropes to an item or to one another in rigging and load securement applications.

What points should be considered while using a shackle?

  • Always check that the shackle is equal to or greater than the Working Load Limit (WLL) of the slings and other rigging gear being utilised.
  • Avoid side loading chain shackles since it may permanently twist or distort the shackle's bow.

What are the types of applications in which shackles are used?

  • Towing or pulling
  • Rigging
  • Hoisting
  • Lifting
  • Tie-down

What are the different parts of a shackle?

  • Bow: It is also known as the body, bail, bowl or dee. It is the curved section of the shackle body opposite the pin.
  • Ear: It is used to hold the shackle pin.
  • Pin: It is the steel bolt which is designed to span the two shackle ears.
  • Shoulder: It is the portion of the pin that rests against the ear when the pin is fully threaded or engaged.

What are the types of shackle bows?

  • Anchor / Bow Shackles
  • Chain / D Shackles

What are the types of shackle pins?

  • Screw Pin Shackles
  • Bolt Shackles
  • Round Pin Shackles

What is Con-Sert Tool #8?

Con-Sert #8 tools are designed for fast & easy installation of concrete screws.

What is a drop-in anchor setting tool?

These tools can be used for hanging pipes and anchoring into concrete. Drill a hole in concrete and insert the anchor into the hole that has already been created.

What is a pilot punch and how is it used?

Pilot punches are used as locating tools for progressive dies. The material is transferred to the following station when a punch creates a hole in one station. Before the press cycles the next stroke, the pilot punch inserts itself into the hole and precisely places the material.

How are female threaded drop-in anchors installed?

  • Drop-in anchors are employed for overhead applications because the interior plug of the anchor stretches in four directions to keep the anchor securely inside the hole before inserting a threaded rod or bolt.
  • To install, set the anchor into the hole, insert the necessary anchor setting tools into the anchor and whack the tool with a hammer until the thicker part of the tool contacts the anchor.
  • When necessary, this kind of mechanism enables you to remove the bolt, but it keeps the anchor in place and concealed in concrete.

What are the important points to remember while installing anchors?

  • Anchors can be positioned flush with the surface or below the surface's base.
  • To support temporary concrete formwork, use anchors that have a coil thread.
  • For easy threading with a corresponding rod or bolt, their threads are shallow and widely spaced.
  • They are not intended to be used permanently.

We are here to help!

Looking for a part not listed here?