Anchor Kits

Filter

SAMMYS -

Installation Kit

ModelItemPrice (ex. VAT)
8122910AC6TPY€354.41
THOMAS & BETTS -

Anchor Kit Containing, 3/4 Inch Size, 12PK

ModelItemPrice (ex. VAT)
51-008BK8XKQ€119.55
THOMAS & BETTS -

Anchor Kit, 12PK

ModelItemPrice (ex. VAT)
51-212HXBK8XKU€124.19
See Details
THOMAS & BETTS -

Anchor Kit, 12PK

ModelItemPrice (ex. VAT)
51-212BK8XKZ€106.03
See Details
THOMAS & BETTS -

Anchor Kit, 12PK

ModelItemPrice (ex. VAT)
51-404HXBK8XLB€91.32
See Details
THOMAS & BETTS -

Anchor Kit, 12PK

ModelItemPrice (ex. VAT)
51-404BK8XLC€92.53
See Details
THOMAS & BETTS -

Anchor Kit, 12PK

ModelItemPrice (ex. VAT)
51-216BK8XLD€188.46
See Details
RED HEAD -

Adhesive Kit, Acrylic Anchoring Type

ModelItemPrice (ex. VAT)
A7P-501KITCG8YQR-
RFQ

Anchor Kits

Anchor kits are made to hold structural and non-structural elements in place for plumbing, construction, maintenance and repair applications by installing anchors in concrete / wooden surfaces.

Frequently Asked Questions

How do anchor kits work?

An object can be hung using screws or nails after using an anchor kit to provide a safe anchor point.

How do I choose the right type of anchor kit?

The right type of anchor kit depends on the type of surface you are working with and the weight of the object you need to hang.

How to ensure safety while using anchor kits?

Wear appropriate eye protection equipment while drilling into any surface.

What are the advantages of an anchor kit over other methods of hanging objects?

Anchor kits provide a more secure hold, which is especially important for heavier objects. They distribute the weight of the object more evenly, reducing the risk of damage to the surface.

How do I know if an anchor kit is the right size for the object I want to hang?

Check the weight limit of the anchor kit and ensure that it is greater than the weight of the object you want to hang.

How do I know if an anchor kit has been installed correctly?

  • The object being hung should be secure and not wobble or move.
  • The anchor should also not be visible or protruding from the surface.

We are here to help!

Looking for a part not listed here?