Air Cocks

Filter

Air cocks are small valves ideal for use in HVAC, plumbing & heating systems, marine applications and more. They control the entrance / escape of air into / from gas lines &...Read more

Air Cocks

Apollo air cocks are designed for controlling the entrance / escape of air into / from gas lines & plumbing systems. These shut-off valves feature brass construction for providing protection against corrosive fluids & mild chemicals while ensuring a contaminant-free operation with applications involving drinking water. They further come equipped with lever / tee type handle for providing maximum user comfort for prolonged use. Choose from a wide variety of these air cocks available in pressure capacities up to 250 psi on Raptor Supplies.

Frequently Asked Questions

How to clean these air cocks?

  • Shut off the valve supplying the air cocks and make sure that there is no pressure in the system.
  • Use a wrench to loosen and remove the air cock from the pipeline or equipment.
  • Soak the air cock in a cleaning solution or solvent that is appropriate for the type of material the air cock is made of. You can use a wire brush or cloth to scrub any dirt, debris or corrosion from the air cock.
  • After soaking the air cock for a period of time specified by the cleaning solution or solvent manufacturer, rinse the air cock thoroughly with clean water.
  • Inspect the air cock for any signs of wear, damage or corrosion. Replace the air cock if it is damaged beyond repair.
  • Before re-installing the air cock, apply a small amount of thread sealant on the threads of the air cock to ensure a tight seal.
  • Tighten the air cock onto the pipeline or equipment with a wrench. Do not over-tighten to prevent damage to the air cock or cause leaks.
  • Turn on the valve supplying the air cocks and check for any leaks or abnormalities in the system.

How do you know if an air cock is clogged?

If an air cock is clogged, you may notice reduced airflow or pressure in the system or it may not vent properly. You may also see visible signs of debris or buildup around the air cock. Clean / replace a clogged air cock to prevent damage to the system.

How often should air cocks be inspected?

Inspect air cocks regularly to ensure their proper functioning and prevent issues, such as clogging or leakage. Consult with a professional to determine the appropriate inspection schedule for your specific application.

We are here to help!

Looking for a part not listed here?