Adhesion Testers

Filter

Adhesion testers measure the force required to pull apart two stuck surfaces. These instruments are commonly used in the automotive, aerospace, construction and packaging industries. They...Read more

DEFELSKO -

Adhesion Tester

ModelItemPrice (ex. VAT)
POSITEST ATAB9XUK€2,983.76
DEFELSKO -

Automatic Coating Adhesion Tester

ModelItemPrice (ex. VAT)
AT-AAE6REX€3,767.24

Frequently Asked Questions

What are the units of force displayed by these units?

Pounds per square inch or Newton per square millimetre.

How to clean the surfaces before performing an adhesion test?

Use a solvent or cleaning solution to clean the surface.

What to do if the force required to separate the surfaces is significantly lower or higher than expected?

If the instrument's readings of the force required to separate the surfaces are significantly lower or higher than expected, it could indicate a problem with the adhesive bond or the bonding process. In such cases, the results of the adhesion test should be used to make adjustments to the bonding process to improve the quality of the adhesive bond.

How to interpret the results of an adhesion tester?

The results of these adhesion testers are reported as a value of adhesive strength. These values can be compared to standards or specifications to determine the suitability of the adhesive or coating for a particular application.

What are the potential sources of error while using an adhesion tester?

The common sources of error include improper tester calibration, variations in the material properties and differences in the surfaces being bonded.

We are here to help!

Looking for a part not listed here?