SAFETY SPEED

Safety Speed catalogue includes panel saws, circular saw blades, belt sanders and accessories. The brand's panel saws provide a safe and fast solution for processing panels. They have heavily guarded saw blades to keep users from unwanted contact. Safety Speed wide belt sanders are available in single and three-phase units and provide a working width of up to 42 inches. Their large belts account for increased capacity, less heat accumulation and fewer belt replacements.

See More

Request a Quote

Product Categories

SAFETY SPEED Belt Sanders

Belt Sanders(4 Products)

SAFETY SPEED Panel Saw Accessories

Panel Saw Accessories(64 Products)

SAFETY SPEED Panel Saws

Panel Saws(21 Products)

SAFETY SPEED Sanding Belts

Sanding Belts(14 Products)

SAFETY SPEED Circular Saw Blades

Circular Saw Blades(12 Products)

SAFETY SPEED Belt/Disc Sanders

Belt/Disc Sanders(2 Products)

SAFETY SPEED Glues

Glues(1 Product)

Things To Consider

Cross-Reference Alternatives

Safety Speed MPNs cross individual references to the equivalent Kett Tools, Milwaukee and Saw Trax model numbers for panel saws and related accessories. So, if you're looking for a competitor item that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Safety Speed products available.

Shipping

These Safety Speed products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.

About Safety Speed

Safety Speed catalogue includes panel saws, circular saw blades, belt sanders and accessories. The brand's panel saws provide a safe and fast solution for processing panels. They have heavily guarded saw blades to keep users from unwanted contact. Safety Speed wide belt sanders are available in single and three-phase units and provide a working width of up to 42 inches. Their large belts account for increased capacity, less heat accumulation and fewer belt replacements.

Major Trade Names

C4 Panel Saws

C4 Panel Saws

These portable frame saws are designed for the accurate and efficient cutting of large sheets of wood, plastic and other materials. They can create maximum 55 inches crosscuts by using adjustable vertical and horizontal rulers. They feature a 4 Nylatron roller bearing system for smooth performance, ...

injection-moulded plastic rollers and a spring-loaded counter-balance system for easy movement and control.

Glue Pot Edgebander

Glue Pot Edgebander

This unit is designed to apply glue to the panel before edgebanding and trimming. It comes integrated with a temperature-controlled Glue Pot that prevents the glue from overheating or splattering. It is equipped with two industrial routers and knives to provide efficient trimming, eliminating the ne...

ed for sanding or filing edges separately. The unit also features a micro-adjust tape guide for making quick changes to tape widths.

MID-WAY FENCE

MID-WAY FENCE

This unit helps to improve the accuracy and precision of table saw cuts by bringing the table to the waist height, thereby reducing back fatigue while cutting small panels. It includes a stop block riding over gauges for quickly setting stops for repeated cuts and durable construction to ensure long...

-lasting durability.

QUICK-STOP Gauge

QUICK-STOP Gauge

This accessory allows adjustable repeat cutting at any length using an 8-foot-long extrusion and an adjustable machined aluminium stop block. It features a convenient thumb screw that allows precise positioning and recessed gauges for making accurate cuts.

Safety Speed Competitive Advantages

SR5 Panel Saw / Router

SR5 Panel Saw / Router

This combination saw / router allows quick cutting or routing applications by quickly changing from a saw to a router in 30 seconds. It comes with a patented self-adjusting router carriage and two dado stops to provide consistent depth of cuts and has an integrated dust collection system for removing dust and debris. They feature an adjustable floa...

ting router head that can be moved up / down for routine grooves, slots and other shapes on wood or other materials.

Frequently Asked Questions

How to operate C4 Panel Saws?

  • Set up the saw by adjusting the height and angle of the blade and the fence, which is the guide that helps to keep the workpiece in place.
  • Also, adjust the blade guard, which is a safety feature that covers the blade and prevents the operator from accidentally touching it.
  • Once the saw is set up, load the sheet of material onto the saw table, making sure it's properly aligned with the fence and the blade.
  • Now turn on the saw and push the material through the blade, using the fence as a guide to ensure a straight cut. During the operation, the saw blade spins at high speed, slicing through the material and creating a smooth, straight edge.
  • Once the cut is complete, the operator removes the cut piece and repeats the process for the remaining sheets of material.

How to maintain Glue Pot Edgebander?

  • Regularly clean the glue pot after each use to prevent the glue from hardening and clogging the nozzle or the heating element.
  • Use a scraper or a brush to remove any excess glue and wipe the pot with a cloth dampened with a solvent or mineral spirits.
  • Always check the adhesive to avoid overheating or burning the glue. Add more glue as needed.
  • Set the glue pot to the correct temperature for the type of adhesive being used. Check the Adjust the heat as needed to ensure that the glue is melted and flowing properly.
  • Inspect the glue nozzle for clogs or other damage that may affect the flow of glue onto the workpiece.
  • The heating element of the glue pot should be cleaned and inspected regularly to ensure that it is functioning properly. Check the wiring and connections for any signs of damage or wear and replace them if needed.

How to adjust the dado stops in the SR5 panel saw / router?

  • Before using the dado stops, install the appropriate blade or bit on the saw / router.
  • Determine the depth of the cut you want to make and adjust the blade accordingly.
  • Once the blade is set to the correct depth, engage the dado stops by sliding them into place. The stops should be positioned in such a manner that the blade comes in contact with the stops at the desired depth.
  • When the stops are properly set up, test the cuts. As the blade reaches the depth of the stops, these stops will engage and prevent the blade from cutting any further.
  • Check the depth and fit of the dado joint to ensure it meets the requirement. If necessary, make adjustments to the blade depth or position the stops correctly to achieve the desired results.