ECLIPSE

The brand's product catalogue includes a wide range of products like crimpers & die sets, hydraulic tools, hole making & punch down tools, screwdrivers & bits, wenches & sockets, power tools, safety gears and other test instruments. Eclipse's wrist straps are a type of wristband that protect from electrostatic discharge (ESD) in sensitive electronic environments. These bands are made of conductive material and have a built-in resistor that allows the strap to provide a controlled path for static electricity to flow while limiting the current to a safe level. They need to be connected to a proper grounding point to effectively dissipate static charges. The brand's punchdown tools are suitable for connecting telecom and data cable to patch panels, wiring blocks, keystone jacks and other network connectors. They feature a sharp blade that pushes or punches down the wire into the IDC contacts, making a reliable connection. They also have an ergonomic profile with a cushioned surface to provide a non-slip grip.

See More

Request a Quote

Product Categories

Things To Consider

Cross-Reference Alternatives

Eclipse Tools MPNs cross individual references to the equivalent Greenlee and Westward model numbers for insulated tool sets, ESD wrist straps and crimping tools. So, if you're looking for a competitor item that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Eclipse Tools items available.

Shipping

These Eclipse Tools products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.

About Eclipse

The brand's product catalogue includes a wide range of products like crimpers & die sets, hydraulic tools, hole making & punch down tools, screwdrivers & bits, wenches & sockets, power tools, safety gears and other test instruments. Eclipse's wrist straps are a type of wristband that protect from electrostatic discharge (ESD) in sensitive electronic environments. These bands are made of conductive material and have a built-in resistor that allows the strap to provide a controlled path for static electricity to flow while limiting the current to a safe level. They need to be connected to a proper grounding point to effectively dissipate static charges. The brand's punchdown tools are suitable for connecting telecom and data cable to patch panels, wiring blocks, keystone jacks and other network connectors. They feature a sharp blade that pushes or punches down the wire into the IDC contacts, making a reliable connection. They also have an ergonomic profile with a cushioned surface to provide a non-slip grip.

Major Trade Names

Pass-Through Mini Crimper

Pass-Through Mini Crimper

This crimper is designed to accommodate modular connectors (RJ45), which have openings on both ends to allow conductors to pass through completely. The tool has two crimping slots, one for the connector's RJ45 plug and another for the cable's outer jacket. This allows for simultaneous crimping of bo...

th the plug and the jacket, ensuring a solid connection and strain relief. It features an ergonomic handle that provides maximum grip with reduced hand fatigue and a ratchet mechanism that releases the handles automatically once the process is complete.

TUFFPUNCH Knockout Punch

TUFFPUNCH Knockout Punch

This hydraulic knockout punch is used to punch precisely sized holes on electrical panels or tough sheet metal as well as flexible materials. It features a lightweight design for fast operation and is designed to deliver up to 6 tons of hydraulic force for easy punching. This knockout punch consists...

of a punch, die, draw stud and a ratchet handle for creating holes in multiple sizes.

Pro-Soft Series Screwdrivers

Pro-Soft Series Screwdrivers

These flat-blade screwdrivers are used for turning or driving screws with a straight slot or groove on top. They feature a moulded propylene handle for a comfortable hold, high-grade chrome vanadium steel for increased toughness and wear resistance. These screwdrivers have an embedded blade portion ...

that has protruding tabs to maintain a secure fit to the handle and provide superior torque performance.

Lunar Series Crimpers

Lunar Series Crimpers

These pin terminal crimpers are designed to attach contact pins to the wire. They feature a controlled-cycle mechanism that ratchets the jaws to crimp to a preset depth and apply a uniform pressure to prevent over-crimping. They come with an elastomeric resin handle for a non-slip grip and high-qual...

ity carbon steel construction for superior durability.

Eclipse Competitive Advantages

Eclipse Tools MultiFinder

Eclipse Tools MultiFinder

This device is suitable for locating edges and centre of the wood, metal studs and joists behind walls, floors and ceilings. It includes features like visual & audible indicators for alerting the user, a three-mode selection with an easy-to-read display and an ergonomic handle for comfortable use. This unit uses a 9V battery (not included) and is c...

apable of detecting depths up to 0.75 inches.

Frequently Asked Questions

How to operate the TUFFPUNCH knockout punch?

  • Select the appropriate punch and die size for the desired hole diameter. Ensure that the punch & die are compatible with the material.
  • Mark the location to create the hole in the material. Use a pencil or marker to make a clear mark.
  • Align the punch and die with the desired location on the material.
  • Insert the draw stud through the punch, die and material.
  • Attach the ratchet handle to the draw stud. Make sure it is tightened securely.
  • Apply steady pressure on the ratchet handle in the clockwise direction. This helps to drive the punch through the material, creating the hole. Keep turning the ratchet handle until the punch fully penetrates the material.
  • Once the punch has cut through the material, release the pressure on the ratchet handle and unscrew the draw stud to remove the punch and die from the hole.
  • Inspect the hole to ensure it is clean and free of burrs or sharp edges. If necessary, use a deburring tool or file to smooth out any rough edges.

How do I properly wear an Eclipse ESD wrist strap?

  • Ensure the wrist strap is properly connected to a grounding system, such as an ESD grounding point or an ESD mat.
  • Place the wristband securely around the wrist, ensuring good skin contact.
  • Adjust the strap for a comfortable fit, ensuring it is not too tight or too loose.
  • Make sure the metal plate or stud on the strap is in direct contact with your skin.
  • Verify that the grounding system is functioning correctly by using an ESD tester or multimeter, if available.

Can I use an Eclipse ESD wrist strap on both wrists simultaneously?

While it is possible to use wrist straps on both wrists simultaneously, it is generally not recommended. The primary purpose of the wrist strap is to provide a controlled path to the ground for static charges. Wearing two wrist straps can create potential differences in grounding, which may lead to improper dissipation of charges and cause damage to the sensitive equipment.